This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3501E: CC3501E device not currently recognized when import example

Part Number: CC3501E
Other Parts Discussed in Thread: CC3501

Tool/software:

Hi admin,

When I import example of CC3501 SDK, CCS has eror: "This project was created for a device not currently recognized - Cortex M.CC35X1.".

CCS version:  20.0.1.4__1.6.1

Please help. Thanks 

  • Hi,

    CC35xx are not supported in CCS yet. There is a step that needs to be done. You can read on the user guide under the ./docs directory of the SDK.

    Basically, it is under ./tools/cc35x1_device_support of the SDK.

    Also, CCS v20 has not been tested. Please use CCS v12.7.1 (this is what I use).

    Shlomi