This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3551E: Questions about CC3551 AT command sample code.

Expert 1135 points
Part Number: CC3551E
Other Parts Discussed in Thread: CC3551

Tool/software:

Hi Ti Experts.

We have a project that has already started.
Need to use AT command set.
I have previously asked TI whether they will release AT command set sample code like CC3235.


So I have two questions.
Q1: When is the expected time to merge the AT command set into the SDK?
Q2: Are most of the AT command set of CC3551 the same as CC3235? If so, we can let customers refer to the command set of CC3235 first.

  • Hello Weli,

    1. We expect top have this later in the year. Today we are focused on enabling all peripheral drivers and network stack integration.

    2. I would assume yes, there is a possibilty that some may not be compatible with the new device, but I expect all commands to be the same.