This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: Using the TI software to connect with the WL1807MOD

Part Number: WL1807MOD


Tool/software:

 I installed the TI software (TI Wireless tool 4.0.0.2) for communicating with the WL1807MOD. So far I am not able to connect to the module. I have taken pictures for the error, but can not find an option to up load the files. Any help will be appreciated.

  • Hello John,

    It would be helpful to get more information on the issue.

    If you look at the bottom of the input box, there is an "insert" button, you can use this to insert code snippets and pictures.

    You can also copy and paste the print out.

    Thanks,

    AB