Part Number: CC3351
Tool/software:
Hello All,
I plan on using CC3351ENJARSBR for one of Display project and i would like to know if the IC supports WiFi-Direct and SDK is available for the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC3351
Tool/software:
Hello All,
I plan on using CC3351ENJARSBR for one of Display project and i would like to know if the IC supports WiFi-Direct and SDK is available for the same.
Hi Jitun,
The CC3351 currently does not support WiFi direct, but is planned to be added later this year.
Are you looking to use CC3351 in a Linux or MCU attached system?
The end system is not yet defined yet, we are still exploring the options of MCU,MPU or a smart module, can you tell me which ICs support wifi direct as of now so that i can start the component selection,
The driver (version 1.0.0.8 via iw phy) reports that P2P is supported, and the supplicant then starts a p2p-dev device.
# iw phy
...
Supported interface modes:
* managed
* AP
* AP/VLAN
* monitor
* P2P-client
* P2P-GO
* P2P-device
valid interface combinations:
* #{ managed, P2P-client } <= 2, #{ AP, P2P-GO } <= 1, #{ P2P-device } <= 1,
total <= 3, #channels <= 2
# iw dev
phy#0
Unnamed/non-netdev interface
wdev 0x2
addr a6:34:f1:b3:23:d4
type P2P-device
Interface wlan0
ifindex 5
wdev 0x1
addr a4:34:f1:b3:23:d4
type managed
Is this not valid?
Hi Jitun,
You can find support for WiFi Direct/P2P in our WL18xxMOD series of devices within linux context:
https://www.ti.com/product/WL1837MOD
But again, it is planned to be supported on the newer CC33xx series.
Hi Dean,
This is correct. The feature exists in the linux driver, but it is not yet implemented in the firmware. Your mileage may vary.