Hi,
Is cdc acm protocol module available on AM1808 logicpd zoom development kit? The linux kernel is 2.6.33-rc4. apparently it is not because when I type
root@am180x-evm:/usr/share# modprobe cdc-acm
FATAL: Module cdc_acm not found.
in the bash, I got the module not found error. Is there anyway to use this class type? do I need to rebuild the kernel?
Thanks,
Sepehr