This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: CC3301 Custom Board Range Test and Packet Error Data.

Part Number: CC3301


Tool/software:

Hi Ti Experts,

We have developed a custom hardware using CC3301 Wi-Fi - BLE combo chipset and we are now in hardware verification stage. We would like to know your comments on two RF test cases.
Hope you will help us on this, please see the following queries :


1) Using the simple link Wi-Fi tool box on two different PC's with our custom boards connected, is it possible to configure one board as transmitter and other as receiver to measure the range and data packet loss at different distances ? 

2) Is there any mobile application available to test range and packet loss between our custom hardware and mobile phone ?

Thanks,
Deepak D.


  • Hi Deepak,

    1) Yes, you can do so since the CC3301 can both transmits or receive data, so I don't see any issue here. A simple setup can be set one device as an AP and the other as a STA, or using RadioTool to have one transmitting (Tx) and the other receiving (Rx).

    2) Sorry but I'm not familiar such applications.

    Let me know if I can further assist you.
    Best regards,

    Omri

  • Hi Deepak,

    2) Is there any mobile application available to test range and packet loss between our custom hardware and mobile phone ?

    You can use iperf to test the overall throughput, and then measure the RSSI signal between the hardware and phone to check the range. 

  • Thanks Sabeeh Khan, I will check.

  • Hi Omri,

    Issue now we are facing is the Radio Tool is not working properly.
    It has issues in giving commands to the custom hardware.
    Please check the log attached.

    [ 3/28/2025, 19:31:30 ] Configuraton loaded successfully
    [ 3/28/2025, 19:31:30 ] Avaliable options loaded successfully
    [ 3/28/2025, 19:31:31 ] Device xds110 reset successfully
    [ 3/28/2025, 19:31:38 ] Device type is LX
    [ 3/28/2025, 19:31:45 ] Device reset successfully
    [ 3/28/2025, 19:31:45 ] Start 2nd Bootloader loading
    [ 3/28/2025, 19:31:46 ] Loaded 18%
    [ 3/28/2025, 19:31:46 ] Loaded 43%
    [ 3/28/2025, 19:31:47 ] Loaded 67%
    [ 3/28/2025, 19:31:48 ] Loaded 86%
    [ 3/28/2025, 19:31:50 ] Loaded 100%
    [ 3/28/2025, 19:31:50 ] Container downloaded successfully
    [ 3/28/2025, 19:31:50 ] Start Firmware loading
    [ 3/28/2025, 19:31:51 ] Loaded 3%
    [ 3/28/2025, 19:31:51 ] Loaded 3%
    [ 3/28/2025, 19:31:52 ] Loaded 7%
    [ 3/28/2025, 19:31:53 ] Loaded 11%
    [ 3/28/2025, 19:31:54 ] Loaded 16%
    [ 3/28/2025, 19:31:55 ] Loaded 20%
    [ 3/28/2025, 19:31:56 ] Loaded 24%
    [ 3/28/2025, 19:31:57 ] Loaded 28%
    [ 3/28/2025, 19:31:58 ] Loaded 33%
    [ 3/28/2025, 19:31:59 ] Loaded 38%
    [ 3/28/2025, 19:32:00 ] Loaded 42%
    [ 3/28/2025, 19:32:01 ] Loaded 46%
    [ 3/28/2025, 19:32:02 ] Loaded 51%
    [ 3/28/2025, 19:32:03 ] Loaded 55%
    [ 3/28/2025, 19:32:04 ] Loaded 59%
    [ 3/28/2025, 19:32:05 ] Loaded 63%
    [ 3/28/2025, 19:32:06 ] Loaded 68%
    [ 3/28/2025, 19:32:06 ] Loaded 72%
    [ 3/28/2025, 19:32:07 ] Loaded 76%
    [ 3/28/2025, 19:32:08 ] Loaded 80%
    [ 3/28/2025, 19:32:09 ] Loaded 85%
    [ 3/28/2025, 19:32:10 ] Loaded 90%
    [ 3/28/2025, 19:32:11 ] Loaded 94%
    [ 3/28/2025, 19:32:12 ] Loaded 98%
    [ 3/28/2025, 19:32:14 ] Loaded 100%
    [ 3/28/2025, 19:32:14 ] Container downloaded successfully
    [ 3/28/2025, 19:32:14 ] Waiting for Firmware to Boot
    [ 3/28/2025, 19:32:15 ] Loaded 100%
    [ 3/28/2025, 19:32:15 ] Container downloaded successfully
    [ 3/28/2025, 19:32:16 ] Loading cc33xx_conf.bin
    [ 3/28/2025, 19:32:18 ] Radio Tool Version  : 2.3.0-rt
    [ 3/28/2025, 19:32:19 ] Device UDID         : 5526-d923-a312-a8
    [ 3/28/2025, 19:32:20 ] FW Version          : cc33xx_rev_1.7.0.237
    [ 3/28/2025, 19:32:22 ] Mac Address         : f8:fb:90:17:f0:fc
    [ 3/28/2025, 19:32:23 ] PHY Version         : 2.40.5.23.68
    [ 3/28/2025, 19:32:23 ] CPE Version         : F20E
    [ 3/28/2025, 19:32:23 ] MCE Version         : 0127
    [ 3/28/2025, 19:32:23 ] PLT Mode Enabled
    [ 3/28/2025, 19:32:24 ] Successfully set antenna to: 0
    [ 3/28/2025, 19:33:56 ] Fail to turn on PLT
    

  • Hi,

    I'm closing this thread since we went to an email communication.

    Best regards,
    Omri