Other Parts Discussed in Thread: LP-EM-CC35X1, , SYSCONFIG, CC3500, CC3501E, ENERGIA
Tool/software:
Hi Team,
I am working on a board based on the LP-EM-CC35X1_RevE3_DesignFiles.
I have received the board and am in the process of bringing up the CC3551E MCU. However, we are unable to find CC35X1 in either SysConfig or Resource Explorer. As a workaround, we are using CC3500 in SysConfig to mimic the MCU, which has been working fine so far—except for I2C1.
According to the datasheets for both CC3501E and CC3551E, I2C1 can be configured to use GPIO3 (SDA) and GPIO2 (SCL). We followed this design guideline, but SysConfig does not provide an option to assign GPIO2 and GPIO3 to I2C1.
Could you confirm whether the datasheet’s information on I2C1 is correct? We are about to begin fabrication of the next revision, and if the datasheet is inaccurate, we will need to make hardware design changes. This is quite urgent as we are facing a project deadline.
Additionally, could you provide the correct SDK for CC3551E and CC3501E, including proper SysConfig support?
Thanks in advance for your help.
Best regards,
Robert