Tool/software:
The INI PowerLimitArray value cannot be set low enough to meet the Korean Channel 48 conducted limit of 4dBm/MHz for RU26 allocations.
Calibrator Tool was used to determine the power setting for compliance where the TX_POWER can be set in the range of -10 to 21 dBm in 1 dB steps.
The minimum INI PowerLimitArray setting I have found that works is 0x01 which corresponds to a TX_POWER setting of 0.5dBm. Note - if the PowerLimitArray setting is 0x00, the device will transmit at max power.
Why is there a disconnect between the Calibration Tool and the INI file for available power settings? How do we call for a lower INI power setting in order to be compliant on this channel in Korea?