This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: WL1837MOD

Part Number: WL1837MOD

Tool/software:

We are using the WL1837MOD for Wi-Fi and Bluetooth in our embedded device. We would like to update our Bluetooth to the latest service package release from here https://www.ti.com/tool/WL18XX-BT-SP. The SP version is wl18xx_bt_sp_v4.8.

According to our Bluetooth Service Pack Update Procedure, we are supposed to open the TIInit_11.8.32.bts file with HCITester and comment out the following lines of code at the end of the BTS file to disable sleep mode. 

The following is an example:

# ----------------- Sleep mode configuration -------------------------------------------------------------

# Sleep mode configuration- default is HCILL sleep protocol

# Send_HCI_VS_Sleep_Mode_Configurations 0xFD0C, 0x00, 0x01, 0x00, 0xff, 0xff, 0xff, 0xff, 0x0064

# Wait_HCI_Command_Complete_VS_Sleep_Mode_Configurations_Event 5000, 0x00, 0xfd0c, 0x00

When I try to open the TIInit_11.8.32.bts file with HCITester I get the following error:

The HCITester version I am using is 3.0.0.37.   Does HCITester support opening the wl18xx_bt_sp_v4.8 version of BTS files? 

Also, when I open the TIInit_11.8.32.bts in hex editor, I don't see the HCI Sleep commands above at the end of the BTS file.  Is the HCILL sleep protocol enabled by default in the SP 4.8 BTS file?