Tool/software:
Hi,
bluetoothctl shows "No default controller available".
because AM62B-P1 doesn't have cc33xx-nvs.bin or another reason?
[ 3.141483] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
[ 3.174552] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.218211] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.224573] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 3.321699] cc33xx_driver cc33xx.5.auto: Direct firmware load for ti-connectivity/cc33xx-nvs.bin failed with error -2
done
Starting system message bus: done
Starting iptables: OK
Starting bluetoothd: OK
Starting network: [ 3.513364] Bluetooth: Core ver 2.22
ifup: don't have all variables for eth0/inet
[ 3.517148] NET: Registered PF_BLUETOOTH protocol family
[ 3.526315] Bluetooth: HCI device and connection manager initialized
[ 3.536674] Bluetooth: HCI socket layer initialized
[ 3.541919] Bluetooth: L2CAP socket layer initialized
Starting telnetd: OK
Welcome to Buildroot
(none) login: root
# calibrator dev wlan0 cc33xx_plt set_manual_calib -rx 1 -tx 1
set_manual_calib has been called with: 4 Parameters
Calibrator:: Setting Calibration Parameters
# ls -l
total 0
# bluetoothctl show
No default controller available
#