This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: STA - Disconnection event, Reason 0x01 ( WLAN_DISCONNECT_UNSPECIFIED )

Part Number: CC3301

Tool/software:

I got an MCU interfacing the CC3301 using last R5 driver version. 

unfortunately, i am facing disconnection event in the driver from the access point i am connect to. This event sometime occure quicly or sometime after 20 minutes so this is quitte hard to reproduce. 

The disconnection event reason is 0x01 so Unspecified ... 

Attached are CC3301 log output. i can see that multicast frames counter is inceasing, could this be the reason ? the driver seem to be unresponsible after the disconnection occure. 


  • [16-06-2025-15:10:03.656] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:485
    [16-06-2025-15:10:03.671] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.679] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:432
    [16-06-2025-15:10:03.687] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.699] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:471
    [16-06-2025-15:10:03.710] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.722] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:432
    [16-06-2025-15:10:03.734] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.746] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:491
    [16-06-2025-15:10:03.753] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.765] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:432
    [16-06-2025-15:10:03.777] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.789] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:495
    [16-06-2025-15:10:03.796] dbg - wlan, driver : trnsf pckt to netx, type: IPV4
    [16-06-2025-15:10:03.808] dbg - wlan, driver : UDP - src: 10.0.0.1, dst: 239.255.255.250, len:423
    [16-06-2025-15:10:04.039] dbg - wlan, driver : trnsf pckt to netx, type: 0x2600
    [16-06-2025-15:10:06.085] dbg - wlan, driver : trnsf pckt to netx, type: 0x2600
    [16-06-2025-15:10:06.085] dbg - wlan, driver : disconnected from access point BSSID: 10:7c:61:3b:82:30 reason: 0x01    <<<<<<<<<<<<<<<<<<
    [16-06-2025-15:10:26.781] net - dhcp_cli, wlan : STAT_STOP
    [16-06-2025-15:10:26.781] net - dhcp_cli, wlan_event : EV_RST
    [16-06-2025-15:10:26.781] net - dhcp_cli, wlan_event :wlan device disconnected from the AP: "myWifiStation",







    31887 3100.943223 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31888 3100.944219 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31889 3101.117036 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31890 3101.257083 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31891 3101.288639 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31892 3101.446972 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31893 3101.541359 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31894 3101.604304 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31895 3101.605781 CC3301 APS_synced on: PS. Role ID: 0
    31896 3101.664971 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31897 3101.776171 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31898 3101.965130 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31899 3102.012701 CC3301 Init diversity params: diversity_enabled = 1, num_of_antennas = 1, default_ant = 0
    31900 3102.187065 CC3301 Init diversity params: diversity_enabled = 1, num_of_antennas = 1, default_ant = 0
    31901 3102.248327 CC3301 Init diversity params: diversity_enabled = 1, num_of_antennas = 1, default_ant = 0
    31902 3102.389494 CC3301 Init diversity params: diversity_enabled = 1, num_of_antennas = 1, default_ant = 0
    31903 3102.393926 CC3301 Init diversity params: diversity_enabled = 1, num_of_antennas = 1, default_ant = 0
    31904 3102.579305 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31905 3102.594262 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31906 3102.768781 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31907 3102.799339 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31908 3103.065174 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31909 3103.081706 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31910 3103.173605 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31911 3103.236519 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31912 3103.315414 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31913 3103.489324 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31914 3103.492325 CC3301 APS_synced on: PS. Role ID: 0
    31915 3103.496840 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31916 3103.692494 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31917 3103.725044 CC3301 Init diversity params: diversity_enabled = 0, num_of_antennas = 0, default_ant = 0
    31918 3108.785486 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31919 3108.787494 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0                                         <<<< Disconnection occure here +-
    31920 3108.787494 CC3301 RX STA role multicast frames counter: 110
    31921 3114.186256 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31922 3114.190251 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31923 3114.190251 CC3301 RX STA role multicast frames counter: 110
    31924 3124.226946 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31925 3124.228966 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31926 3124.228966 CC3301 RX STA role multicast frames counter: 110
    31927 3134.162441 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31928 3134.165950 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31929 3134.165950 CC3301 RX STA role multicast frames counter: 110
    31930 3144.210563 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31931 3144.212611 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31932 3144.214020 CC3301 RX STA role multicast frames counter: 110
    31933 3154.189929 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31934 3154.193929 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31935 3154.193929 CC3301 RX STA role multicast frames counter: 110
    31936 3164.207478 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31937 3164.209462 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31938 3164.209462 CC3301 RX STA role multicast frames counter: 110
    31939 3174.165306 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31940 3174.167312 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31941 3174.168311 CC3301 RX STA role multicast frames counter: 110
    31942 3184.220606 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31943 3184.222606 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31944 3184.222606 CC3301 RX STA role multicast frames counter: 110
    31945 3194.262262 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31946 3194.266772 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0
    31947 3194.266772 CC3301 RX STA role multicast frames counter: 110
    31948 3204.134714 CC3301 ScanModule_ConfigProbeReqIEs: IEs len 0 exceeds limit 0
    31949 3204.136224 CC3301 TX status counter: fail count: 0x0, expiry count:0x80, exchange count:0x0

  • HEllo,

    Can you share the AP model and settings?
    Can you also try and get FW logs out of the LOG pin?

    We will be releasing a new version in the next 2 weeks which will include many stability and general bug fixes with improved error logging capabilities also.

  • Hello, 

    thanks for your response. 


    the log output bellow is a capture of when the moment error occurs

    AP is a Asus router with WIFI secur mode in WPA3 mode. 

  • Do you know when a final release is expected for firmware ? 
    thanks

  • Let's get you past the scan issue on the other thread and see if you still see this issue on R7.
    If it is let's re open a new thread for R7, I am hopeful we can get you resolution.