Other Parts Discussed in Thread: CC-DEBUGGER
Tool/software:
I 'm using the CC2541 with using the internal voltage for Vref.
I am inputting the output from the AD8497(ANALOG DEVICES) into the AD converter on the CC2541.
A type K thermocouple is connected to the AD8497.
When I connect the CC-DEBUGGER to the CC2541 and check the results, the measurement point is 200°C, but the output temperature is 207°C.
When I use an external voltage of 1.24V instead of the internal voltage for Vref, I can correctly measure 200°C.
The internal voltage for Vref should be specified as 1.24V in the product specifications, but it seems to be operating at 1.21V.
Why is this happening?