This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODSF: Connect a CC3235MOD device to a Windows11 PC

Part Number: CC3235MODSF

Tool/software:

I am trying to connect a CC3235MOD device to a Windows 11 PC using Wi-Fi Direct, but the connection has not been successful so far. Has there been any verified example or case where CC3235MOD was successfully connected to a Windows 11 host via Wi-Fi Direct? On the Windows 11 side, I can see the network name (SSID) being broadcast by the CC3235MOD, but when I try to connect, it prompts me to enter a PIN code. Are there any specific settings or configurations required on the CC3235MOD to enable a successful Wi-Fi Direct connection with Windows 11?

  • Hi Yuji, thank you for your question. With regards to the PIN code, according to page 69 of the Network Processor Manual, there are configurations that can be set for the negotiation method by security types including push button and pin code setups. You may be able to figure out what PIN code to enter if it matches the .Key attribute that you set for the security parameters.

    Surrounding pages of the one I mentioned include some code snippets that may help you as well.

    I hope this helps.