This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: CC3301 - R7 Firmware, WLAN_EVENT_FW_CRASH after a scan request

Part Number: CC3301


Tool/software:

Hello, 

we have just updated from R5 to R7 our driver for the CC3301 but is seem to break what was working. 

The firmware upload properly but as soon as we request a scan we receive a WLAN_EVENT_FW_CRASH event.

I atteched the log output, it seem their is no crash message on it.

thanks for your support

log_cc3301_r7.txt

  • Here is Report output msg :
    FwEvent_CallHandlers: GENERAL ERROR event received! FW is stuck
    wlan unexpected event [0x14

  • can you confirm this is the expected boot output :???

    15017 8471.358342 CC3301 bmTransport_Receive: Processing chunk of size 768
    15018 8471.358342 CC3301 bmTransport_Receive: Processing chunk of size 768
    15019 8471.358342 CC3301 bmTransport_Receive: Processing chunk of size 768
    15020 8471.359389 CC3301 bmTransport_Receive: Processing chunk of size 768
    15021 8471.359389 CC3301 bmTransport_Receive: Processing chunk of size 768
    15022 8471.359389 CC3301 bmTransport_Receive: Processing chunk of size 768
    15023 8471.360342 CC3301 bmTransport_Receive: Processing chunk of size 760
    15024 8471.360342 CC3301 bm_record_receive: Record validation success
    15025 8471.570800 CC3301 First Compare: Scrambled magic number is: 0x35
    15026 8471.570800 CC3301 First Compare: Set timeout to: 3808 uSec
    15027 8471.570800 CC3301 First Compare: First Compare result: 0x11
    15028 8471.570800 CC3301 System Info 0x7F: Set to 0x7F
    15029 8471.570800 CC3301 First Compare: Scrambled magic number is: 0xdd
    15030 8471.570800 CC3301 First Compare: Set timeout to: 3808 uSec
    15031 8471.570800 CC3301 First Compare: First Compare result: 0x11
    15032 8471.570800 CC3301 First Compare: Scrambled magic number is: 0x88
    15033 8471.570800 CC3301 First Compare: Set timeout to: 3808 uSec
    15034 8471.571801 CC3301 First Compare: First Compare result: 0x11
    15035 8471.571801 CC3301 First Compare: Scrambled magic number is: 0xc6
    15036 8471.571801 CC3301 First Compare: Set timeout to: 3808 uSec
    15037 8471.571801 CC3301 First Compare: First Compare result: 0x11
    15038 8471.571801 CC3301 First Compare: Scrambled magic number is: 0xbd
    15039 8471.571801 CC3301 First Compare: Set timeout to: 3808 uSec
    15040 8471.571801 CC3301 First Compare: First Compare result: 0x11
    15041 8471.571801 CC3301 nabHostIf_CommandCompleteCodeDownloadSend: Allocation failed
    15042 8471.571801 CC3301 First Compare: Scrambled magic number is: 0xd0
    15043 8471.571801 CC3301 First Compare: Set timeout to: 3808 uSec
    15044 8471.571801 CC3301 First Compare: First Compare result: 0x11
    15045 8472.589270 CC3301 bleOsprey HwiP_post error 128

  • This is log output after command scan is sent: 

    ...
    15046 8799.711167 CC3301 bleOsprey HwiP_post error 128
    15047 8813.030796 CC3301 presence observer CB. role id 0 is being stopped. exit
    15048 8813.030796 CC3301 presence observer CB. role id 3 is being stopped. exit
    15049 8813.030796 CC3301 presence observer CB. role id 7 is being stopped. exit
    15050 8813.030796 CC3301 presence observer CB. role id 5 is being stopped. exit
    15051 8813.030796 CC3301 Dispatch_RoleDisable

  • Hi Julien,

    Are you using the network terminal example as is, or is this your own implementation?

    Can you upload the logger file in wireshark format, it is easier for us to analyze this way.

    If you have your own application, can you show us how you prep for a scan command?