Other Parts Discussed in Thread: WL1837MOD
Tool/software:
- 5.2.5 – Fail: The test case was ran three times and all three times failed at step 3. The throughput was too low.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
Please find the attached log.
We generated the wl18xx-conf.bin.
=================================
root@s40-bigbend-v1:/lib/firmware/ti-connectivity# sh configure-device.sh --version
Version 1.4
=====================
configure-device.sh Branch details:
SRC_URI = "git://git.ti.com/wilink8-wlan/18xx-ti-utils.git;protocol=https;branch=master"
SRCREV = "7325bf0b7b2d462e334437d2c7f9198d0ac55ce2"
====
root@s40-bigbend-v1:/lib/firmware/ti-connectivity# sh configure-device.sh
Please provide the following information.
Are you using a TI module? [y/n] : y
What is the chip flavor? [1801/1805/1807/1831/1835/1837 or 0 for unknown] : 1807
Should Japanese standards be applied? [y/n] : y
How many 2.4GHz antennas are fitted? [1/2] : 1
How many 5GHz antennas are fitted (using 2 antennas requires a proper switch)? [0/1/2] : 1
Should SISO40 support be applied? [y/n] : y
Regards,
Viswa
Hi,
We have changed the antenna usage to 2 as shown below ,
we are planning to give this bin file for testing. let us know if there is any issue
root@s40-bigbend-v1:~# cd /usr/sbin/wlconf/
root@s40-bigbend-v1:/usr/sbin/wlconf# sh configure-device.sh
Please provide the following information.
Are you using a TI module? [y/n] : y
What is the chip flavor? [1801/1805/1807/1831/1835/1837 or 0 for unknown] : 1807
Should Japanese standards be applied? [y/n] : y
How many 2.4GHz antennas are fitted? [1/2] : 2
How many 5GHz antennas are fitted (using 2 antennas requires a proper switch)? [0/1/2] : 2
---------------------------------------------------------
The device has been successfully configured.
TI Module: y
Chip Flavor: 1807
Base INI file used: /usr/sbin/wlconf//WL1837MOD_INI_FCC_CE_JP.ini
Number of 2.4GHz Antennas Fitted: 2
Number of 5GHz Antennas Fitted: 2
Diversity Support: y
SISO40 Support: y
Japanese Standards Applied: y
---------------------------------------------------------
============================
Also WFA testing team said , they are ready to change the station for debugging purpose only but
For official certification, the Realtek station has to be used.
Regards,
Viswa