This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1271 cal and MAC address

Other Parts Discussed in Thread: WL1271

We are using the WL1271 in a Murata module. We did not realize the Murata did not have a MAC address.

The operating system is Win CE. We are going to run ticon,exe with the following commands:

/w p 1 l2 f2

/trh07

/tbb 375 128 0

/tbt 10000000

This should cal the module and generate the NVS_map.bin file with cal values and the default MAC.

We will then change the MAC address and storage this file in NAND memory.

Is this the only cal we need to do?

Can we run the cal using ticon.exe with a script file using software on the initial board bring up?

If we could we could eliminate a step in our board initializations.

Thanks,

John Moody PTI