Tool/software:
Hi,
WFA - SAE-5_9_1 Ping test case Failed:
wpa_supplicant.conf file has the sae_pwe=2
Tool/software:
Hi,
WFA - SAE-5_9_1 Ping test case Failed:
wpa_supplicant.conf file has the sae_pwe=2
Hi Shlomi,
When I issue the below command from the putty console , I don’t see the IP is getting assigned by the router.
sta_set_ip_config,interface,wlan0,dhcp,1,type,1
We don’t have the dhcp package, we have only dhcpd. I have updated the details same in the ticket.
message sta_set_ip_config,interface,wlan0,dhcp,1,type,1
51
last 0 last-1 0 last-2 0 last-3 0
Inside the CLI huck block
After File open
Outside the new block
sta_set_ip_config
interface wlan0
dhcp 1
type 1
sent to DUT
entering wfaStaSetIpConfig ...
new event
received from DUT
tag 11
status,COMPLETE
status,COMPLETE
root@s40-bigbend-v1:/lcc/data/test_engine# dhcp
sh: dhcp: command not found
root@s40-bigbend-v1:/lcc/data/test_engine#
Regards,
Viswa
Hi,
But it is not the dhcp command that needs to be run.
dhcp is just an argument of the command that it is processing.
And the above does seem as it is applied with no error.
If I take as an example another test that used this command (with different parameters), I see also a good response:
message sta_set_ip_config,interface,wlan0,dhcp,0,ip,192.165.100.111,mask,255.255.0.0 79 last 0 last-1 0 last-2 0 last-3 0 Inside the CLI huck block After File open Outside the new block sta_set_ip_config interface wlan0 dhcp 0 ip 192.165.100.111 mask 255.255.0.0 sent to DUT entering wfaStaSetIpConfig ... new event received from DUT tag 11 status,COMPLETE status,COMPLETEAnd in this case, I see an error of 'no such file or directory'.
message sta_set_ip_config,interface,wlan0,dhcp,1,type,1 50 last 0 last-1 0 last-2 0 last-3 0 Inside the CLI huck block After File open Outside the new block sta_set_ip_config interface wlan0 dhcp 1 type 1 sent to DUT entering wfaStaSetIpConfig ... cp: cannot stat '/etc/resolv.conf': No such file or directory new event received from DUT tag 11 status,COMPLETE status,COMPLETE
Shlomi
Hi Shlomi,
I was able to reproduce the no such file or directory issue. This issue happens only on the first time dont know know why?
Actually, it is the link in S40.
root@s40-bigbend-v1:/lcc/data/test_engine# ls -l /etc/resolv.conf
lrwxrwxrwx 1 root root 18 Mar 9 2018 /etc/resolv.conf -> ../run/resolv.conf
root@s40-bigbend-v1:/lcc/data/test_engine# [ 1142.680331] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
new event
status,RUNNING
message sta_set_ip_config,interface,wlan0,dhcp,1,type,1
51
last 0 last-1 0 last-2 0 last-3 0
Inside the CLI huck block
After File open
Outside the new block
sta_set_ip_config
interface wlan0
dhcp 1
type 1
sent to DUT
entering wfaStaSetIpConfig ...
cp: cannot stat '/etc/resolv.conf': No such file or directory
new event
received from DUT
tag 11
status,COMPLETE
status,COMPLETE
[ 1172.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1202.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1197
[ 1232.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1262.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1292.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1322.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1352.680330] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1197
[ 1382.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1412.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1442.680329] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1472.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1197
[ 1502.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1532.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
[ 1562.680327] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1198
root@s40-bigbend-v1:/lcc/data/test_engine# ls -l /etc/resolv.conf
lrwxrwxrwx 1 root root 18 Mar 9 2018 /etc/resolv.conf -> ../run/resolv.conf
root@s40-bigbend-v1:/lcc/data/test_engine# [ 1592.680328] ili9881c-dsi 5a000000.dsi.0: TE pulse count observed is 1197
new event
status,RUNNING
message sta_set_ip_config,interface,wlan0,dhcp,1,type,1
51
last 0 last-1 0 last-2 0 last-3 0
Inside the CLI huck block
After File open
Outside the new block
sta_set_ip_config
interface wlan0
dhcp 1
type 1
sent to DUT
entering wfaStaSetIpConfig ...
new event
received from DUT
tag 11
status,COMPLETE
status,COMPLETE
Regards,
Viswa
================================
Hi Shlomi,
From the share console putty log, we can see that the ip address is not assigned to the wlan0 interface.
uccl log i could see the ip address is not passed. How the DUT will get the ip address?
2025-07-24 15:13:00.894 - INFO - DUT (192.168.250.111:9000) ---> sta_set_ip_config,interface,wlan0,dhcp,1,type,1
2025-07-24 15:13:01.947 - INFO - DUT (192.168.250.111:9000) <-- status,COMPLETE
wlan0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500 metric 1
inet6 fdc7:4370:cc2a:0:661c:10ff:fe36:2dab prefixlen 64 scopeid 0x0<global>
inet6 2001:db8:100:f101:661c:10ff:fe36:2dab prefixlen 64 scopeid 0x0<global>
inet6 fd0e:993c:9d1d:0:661c:10ff:fe36:2dab prefixlen 64 scopeid 0x0<global>
inet6 fe80::661c:10ff:fe36:2dab prefixlen 64 scopeid 0x20<link>
inet6 fd19:b28f:9007:0:661c:10ff:fe36:2dab prefixlen 64 scopeid 0x0<global>
inet6 fd18:401:85a3:0:661c:10ff:fe36:2dab prefixlen 64 scopeid 0x0<global>
ether 64:1c:10:36:2d:ab txqueuelen 1000 (Ethernet)
RX packets 112 bytes 8550 (8.3 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 23 bytes 2651 (2.5 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
Regards,
Viswa
Hi,
seems like the 1st step of recording the GTK and IGTK is OK when comparing to the supplicant log. Then, connection is succeeded but I do not see DHCP request from the device. This is why PING fails. you can always set is statically on the platform CLI just for the test (e.g. ifconfig wlan0 x.x.x.x).
Can you double check that you do not get an IP address by typing ifconfig and see?
Regards,
Shlomi
Please share me the dhcp bin file to get the ip address? we dont have dhcp package.
root@s40-bigbend-v1:/lcc/data/test_engine# dhcpc
-sh: dhcpc: command not found
root@s40-bigbend-v1:/lcc/data/test_engine# dhcp
dhcp_release dhcpcd
root@s40-bigbend-v1:/lcc/data/test_engine# dhcp
Regards,
Viswa
Hi,
I shared this topic over Email with ways to set the static IP.
We also do not use DHCP since it is not implemented in the agent.
In parallel, I am trying to see if we can add it to the agent.
So you can proceed with setting the expected IP address in systemd and test.
Shlomi
Hi Shlomi,
We have shared the log from the reference unit.
2262.reference-run-PMF-QT-26aug2025.zip7043.reference-run-FC-SAE-27aug2025.zip
Regards,
Viswa
Hi Shlomi,
From the testing team has asked to look at the M3 packet of the eapol to get the IGT_key.
I could not decrypt the wpa_key_data to check for the IGT_KEY_data?
Please let me know how to decrypt ?
Regards,
Viswa
Hi,
This is a WPA3 connection so it is a little more complicated.
You can look at the supplicant log and fetch the PMK.
Then in Wireshark, go to where you add the keys and add it.
You should start seeing the decryption data but for some reason it does not always show the decryption of the EAPOL M3.
Shlomi