Tool/software:
The following description can be found In the document:《 Technical Reference Manual CC35xx SimpleLink Wi-Fi 6 and Bluetooth® Low Energy Wireless MCU 》 2.2 Introduction
• On chip memories – over 1MB SRAM for application data
The definition of the "link.cmd" for the example "CC35xx_network_terminal" is as follows:
MEMORY
{
FLASH_INT_VEC (RWX) : origin = 0x10000000, length = FLASH_INT_VEC_SIZE //0x10000000-0x10001300 0x4kbyte
FLASH_NON_SECURE (RX) : origin = end(FLASH_INT_VEC) , length = build_linker_toolbox_FLASH0_SIZE-FLASH_INT_VEC_SIZE
//FLASH_SECURE (RX) : origin = 0x14000000, length = 0x03FFFFFF //0x14000000-0x17FFFFFF
//INT_VEC (RWX) : origin = 0x00000000, length = 0x000002FF //0x00000000-0x000002FF 0x300kbyte
TCM_CRAM_NON_SECURE (RWX) : origin = 0x00000000, length = 0x00007FFF //0x00000000-0x000007FF 32kbyte
//TCM_CRAM_SECURE (RWX) : origin = 0x04000000, length = 0x03FFFFFF //0x04000000-0x07FFFFFF
CRAM_NON_SECURE (RWX) : origin = 0x08000000, length = 0x0000FFFF //0x08000000-0x0800FFFF 64Kbyte
//CRAM_SECURE (RWX) : origin = 0x0C000000, length = 0x03FFFFFF //0x0C000000-0x0FFFFFFF
TCM_DRAM_NON_SECURE (RW) : origin = 0x20000000, length = 0x0001FFFF //0x20000000-0x2001FFFF 128Kbyte
//TCM_DRAM_SECURE (RW) : origin = 0x24000000, length = 0x03FFFFFF //0x24000000-0x27FFFFFF
DRAM_NON_SECURE (RW) : origin = 0x28000000, length = 0x00037FFF //0x28000000-0x28037FFF
CONNECTIVITY_SHARED_MEM (RW) : origin = 0x2803FF00, length = 0x000000FF //0x2803FF00-0x2803FFFF
//DRAM_SECURE (RW) : origin = 0x2C000000, length = 0x03FFFFFF //0x2C000000-0x2FFFFFFF
/* Explicitly placed off target for the storage of logging data.
* The ARM memory map allocates 1 GB of external memory from 0x60000000 - 0x9FFFFFFF.
* Unlikely that all of this will be used, so we are using the upper parts of the region.
* ARM memory map: https://developer.arm.com/documentation/ddi0337/e/memory-map/about-the-memory-map*/
LOG_DATA (R) : origin = 0x90000000, length = 0x40000 /* 256 KB */
LOG_PTR (R) : origin = 0x94000008, length = 0x40000 /* 256 KB */
}
I think TCM_DRAM_NON_SECURE is the RAM area used by the user.And the TCM_DRAM_NON_SECURE is defined with a size of only 128K, and its content is as follows:
TCM_DRAM_NON_SECURE (RW) : origin = 0x20000000, length = 0x0001FFFF //0x20000000-0x2001FFFF 128Kbyte
May I ask, how should I correctly increase the RAM for this application?