Are the below assumptions correct if the follwoing pins are not planned to be used on the WL1271 based TiWi module?
- Pin 33 AUD_FSYNC Says its a DIO. I am pulling it low.
- Pin 37 AUD_CLK Says its an output so I left it as a NC
- Pin 38 AUD_OUT Says its an output so I left it as a NC
- Pin 40 AUD_IN Says its an input. I am pulling it low.
- Pin 41 BT_FUNC2 Says its an input. I am pulling it high.
- Pin 42 BT_FUNC4 Says its an output so I left it as a NC
- Pin 2 BT_FUNC5 Says its an output so I left it as a NC