Tool/software:
Hello TI Experts,
I am working with the CC3551E device. From the datasheet, I see that it supports dual-band Wi-Fi 6 (2.4 GHz and 5 GHz, single-stream 20 MHz channels) and can operate in roles such as STA, softAP (up to 4 stations), Wi-Fi Direct, and multi-role (AP + STA).
My question is:
Is it possible for the CC3551E to advertise AP on 2.4 GHz and 5 GHz at the same time (concurrent dual-band AP), or does the device only support one band at a time since it is a single-stream radio?
I want to confirm this behavior with an official response/documentation reference.
Thank you.
SDK :simplelink_wifi_sdk_9_13_01_04_ea
Toolbox : simplelink_wifi_toolbox_win_3_1_12
Thank you.