CC3351: OTP and MAC address programming, part II

Part Number: CC3351

Tool/software:

Hello TI,


I was able to get the newer release of CC33XX Linux image on the BeagleBone Black with the CC3351.  wlan0 and hci0 interfaces are brought up, so the CC3351 is connected.

I can now see several new commands listed in calibrator --help.

I have toggled PLT successfully, so the CC3351 is communicating.

However, I am still having trouble flashing OTP using the following command:

root@am335x-evm:~# calibrator wlan0 cc33xx_plt set_efuse -mac_addr 00:11:22:33:44:55 -token <censored>
ERROR: Invalid command

I am wondering if I might have missed something in order to flash the MAC address to OTP.

Thanks,

Edward