LP-EM-CC35X1: simplelink wifi toolbox getting started

Part Number: LP-EM-CC35X1

Tool/software:

Hello,

Just a thought on making the out of box experience for LP-EM-CC35X1 easier, the users guide for the EVM doesn't mention the activation process with WiFi toolbox. It does mention that wifi toolbox is a GUI used for programming the CC35xx but you don't see anything on out of the box how do you set the device up for programming etc. Maybe a link to the quickstart guide here would be helpful.

Also, can we add a label to the crystal selection table for something like:

40 MHz (E2 Launchpad)

52 MHz (E3 Launchpad)

So there's no confusion on which is which?

Similarly love that there's more flash device support options, but the tool should tell you which one is default on the Launchpad just so you don't have to refer back to the quick start guide or some other documentation.

Just a couple thoughts on quality of life improvements here!

Munan