Hi,
I’m working with the TI WL18xx (WiLink 8) module and using the Bluetopia stack with SS1Tool.
I need clarification on configuring BLE connection parameters using HCI_LE_Connection_Update.
1. Connection Timeout / Supervision Timeout
- 
How can I set the connection timeout (or supervision_timeout) through SS1Tool? 
- 
Is the supervision_timeout field equivalent to the BLE connection timeout? 
- 
Can this command be issued directly using SS1Tool, and what is the correct syntax or format? 
2. Recommended Parameter Values
What are the recommended (idle/default) or TI-suggested values for stable BLE connections on WL18xx, particularly for:
- 
conn_min_interval
- 
conn_max_interval
- 
supervision_timeout
3. Example SS1Tool Command to set BLE connection parameters