Hi All,
We are currently working on IMX95 to integrate with CC33xx module.
Details:
Linux Kernel : 6.6
CC33XX Mod with 6.6 patches from TI, to Integrate on IMX95.
SDIO lines are also probed.
---
Required dts and Kernel config changes are built and loaded the image on the IMX95, here is the below screen with the observations:

Here are the SDIO lines info:



Please analyse the inputs given and let us know the further proceeding on this topic.
Thanks,
Satya.