Device : NXP IMX91 SOM From Boundary Devices , Ezurio
OS : Yocto Linux Scarthgap
WiFi/BLE Module : Sona TI351 WiFi6 + Bluetooth v5.4
FW : summit-ti351-WW-firmware-13.24.0.20.tar.bz2 inside https://github.com/Ezurio/Connectivity_Stack_Release_Packages/releases/
Bluez : v5.82
root@nitrogen91:~# hciconfig -a
hci0: Type: Primary Bus: UART
BD Address: E8:CB:F5:80:B9:E9 ACL MTU: 255:10 SCO MTU: 0:0
UP RUNNING
RX bytes:4487 acl:44 sco:0 events:339 errors:0
TX bytes:2965 acl:44 sco:0 commands:284 errors:0
Featur[ 9288.776557] Bluetooth: hci0: unexpected cc 0x0c14 length: 1 < 249
es: 0x00 0x00 0x00 0x00 0x60 0x00 0x00 0x00
Packet type: DM1 DH1 HV1
Link policy:
Link mode: PERIPHERAL ACCEPT
Can't read local name on hci0: Input/output error (5)
I have few Questions :
1. Why is MTU Limited to 255 ?? On other devices , we have higher MTU of 1024
2. Why those errors like "Cant Read Local Name" ??