CC3235MODASF: KC Certification

Part Number: CC3235MODASF

Hi team,

Our communication product include a TI CC3235MODASF module, and our KOREA team is prepareing KC certification process.

Does CC3235MODASF module has any plans to obtain KC certification in the future? 

Or Do you have any experience about this process? 

 

Thanks 

kyrin 

  • No we don't have any plans to pursue KC Certification for CC3235MODASF. I suggest working with an accredited test house to aid your pursuit of this certification.

    Best,

    Josh

  • Hi Josh, 

    Thanks for your help.  We have consulted with a KC certification laboratory. The laboratory informed us of the documents required for the module certification process. The laboratory requires us to provide the supporting documents for the following requirements.

    The RF transceiver module, which is a wireless transmission and reception component of broadcasting and communication equipment, shall meet the following requirements:

    1. The high-frequency section (including parts such as the high-frequency oscillator, high-frequency amplifier, high-frequency mixer, high-frequency modulator, and high-frequency filter) shall have its own electromagnetic shielding structure.
    2. It shall include a data input stage (such as a buffer) that ensures compliance with the Radio Equipment Regulations, even when excessively high-speed data is input.
    3. It shall have a built-in voltage regulation circuit or be designed to receive only a regulated power supply from the final product.
    4. The antenna shall either be permanently connected (non-detachable) or have a connector that allows proper impedance matching.
    5. It shall allow measurement as a standalone unit or have a connector that enables impedance matching with the antenna.
    6. The RF transceiver module shall comply with the relevant technical standards.

    May I ask if TI can help provide the above-mentioned documents or how to obtain them?

    Thanks a lot!

  • Hi Kyrin,

    Happy New Year! Our module complies to the above comments. Do you need access to our reports? You should be able to use our FCC certification reports to help with some parts your system certification process. Please take a look on SIMPLELINK-CC3XXX-CERTIFICATION page and grab our CC32XX-REPORTS. There you should be able to find the reports for your desired module which you can submit to your test house.

    Let me know if there is anything else I can assist with.

    Best,

    Josh

  • Hi Josh,

    Happy New Year, too ! Thanks for your reply. I have download file"CC3235MOD_Cert_Reports_5_20_00_00.zip".

    I have read the content of the report, and it is basically all about the performance compliance tests of wireless radio frequency.

    This seems to be inconsistent with the document I require. In my understanding, the laboratory needs to provide more detailed verification documentation for the module, including its circuit structure, the types of electronic components used, and the compatibility between these components.

    Kind regards

    Kyrin

  • Hey Kyrin,

    Happy New Year! Apologies for the delay here. Can you ask your test house what specifically they are looking for? I understand the comments above, but to me they just list the descriptions of the requirements and not what is need to fulfill them (BOM, PCB Layer Plots, Pictures of the module, etc.)

    Please let me know how I can further assist you :)

    Best,

    Josh

  • Hey Josh,

    After we discussed with KC testing laboratory, we confrim that the following documents are required:

    • BOM : to provide the evidence that the module with include high-frequency electronic components.
    • Schematic: to provide the evidence that the module have a built-in voltage regulation circuit.
    • Chip Architecture Design or date flowchart: A flowchart describing the data input stage for compliance with the Radio Equipment Regulations.

    The above three requirements, maybe BOM and Schematic are clearly, but i don't know what documents can cover the third requirement(marked with blue). So I hope you can help me obtain these three documents.

    Kind regards,

    Kyrin

  • Hey Kyrin,

     Yes that 3rd bullet is not clear... but will take a shot at assuming what they mean :). I am attaching the BOM, SCH, and Device Block Diagram here:

                                 Texas Instruments
    									  
    Current Date/Time: 2019/11/22 09:45:27                               PIN: 63
          Spec Device: CC3235MODASF12MON                                  PKG: MON
             Revision: A                                           PKG Group: QFM
                        
                                                                                     
                                                                                       
    Mount                                                                              
       Incoming IC            : HYBCC3235SF12R                                      01 
       Resistor               : SID#5B-62-1154G                                     01 
          Descriptor          : RES C SMD 0201 100Kohm 5% GP/HF                        
          Supplier            : WALSIN                                                 
          Supplier Number     : WR02X104JAR                                            
          Value               : 100Kohm                                                
          Max Rating          : 1/20W                                                  
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       Resistor Qty           : 8                                                   01 
       RF Switch              : SID#5B-61-0419G                                     01 
          Descriptor          : RF Switch                                              
          Supplier            : Richwave                                               
          Supplier Number     : RTC6608OSP                                             
          Value               : 6GHz                                                   
          Size                : 1.0*1.0*0.4                                            
       Capacitor              : SID#5B-63-1013G                                     01 
          Descriptor          : CAP CER 4.7uF 20 6.3V SMD 0402 GP X6S                  
          Supplier            : TAIYO YUDEN                                            
          Supplier Number     : JMK10SID#5BC6475MV-F                                   
          Value               : 4.7uF                                                  
          Max Rating          : 6.3V                                                   
          Tolerance           : 20                                                     
          Size                : 0402                                                   
       Capacitor              : SID#5B-63-1073G                                     02 
          Descriptor          : CAP CER 4.7uF 20% 6.3V SMD 0402 GP X6S                 
          Supplier            : Yageo                                                  
          Supplier Number     : CC0402MRX6S5BB475                                      
          Value               : 4.7uF                                                  
          Max Rating          : 6.3V                                                   
          Tolerance           : 20%                                                    
          Size                : 0402                                                   
       Capacitor Qty          : 3                                                   01 
       Capacitor 2            : SID#5B-63-1076G                                     01 
          Descriptor          : CAP CER 7.5pF 5% 50V SMD 0201 GP/HF NPO                
          Supplier            : MURATA                                                 
          Supplier Number     : GJM0335C1E7RSID#5BB01D                                 
          Value               : 7.5pF                                                  
          Max Rating          : 50V                                                    
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       Capacitor 2            : SID#5B-63-1100G                                     02 
          Descriptor          : CAP CER 7.5pF  /-0.1pF 25V C0G 0201 SMD                
          Supplier            : Yageo                                                  
          Supplier Number     : CQ0201BRNPO8BN7R5                                      
          Value               : 7.5pF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 2 Qty        : 1                                                   01 
       Capacitor 3            : SID#5B-63-1085G                                     01 
          Descriptor          : CAP CER 22pF 5% 50V SMD 0201 GP/HF NPO                 
          Supplier            : Yageo                                                  
          Supplier Number     : CC0201JRNPO9BN220                                      
          Value               : 22pF                                                   
          Max Rating          : 50V                                                    
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       Capacitor 3            : SID#5B-63-1029G                                     02 
          Descriptor          : CAP CER 22pF 5% 50V SMD 0201 GP/HF NPO                 
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1H220JA01D                                     
          Value               : 22pF                                                   
          Max Rating          : 50V                                                    
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       Capacitor 3 Qty        : 2                                                   01 
       Capacitor 4            : SID#5B-63-1016G                                     01 
          Descriptor          : CAP CER 22uF 20% 4V SMD 0603 GP/HF X6S                 
          Supplier            : Murata                                                 
          Supplier Number     : GRM188C80G226ME15D                                     
          Value               : 22uF                                                   
          Max Rating          : 4V                                                     
          Tolerance           : 20%                                                    
          Size                : 0603                                                   
       Capacitor 4            : SID#5B-63-1071G                                     02 
          Descriptor          : CAP CER 22uF 20% 4V SMD 0603 GP/HF X6S                 
          Supplier            : Taiyo Yuden                                            
          Supplier Number     : AMK107BC6226MA                                         
          Value               : 22uF                                                   
          Max Rating          : 4V                                                     
          Tolerance           : 20%                                                    
          Size                : 0603                                                   
       Capacitor 4 Qty        : 2                                                   01 
       Capacitor 5            : SID#5B-63-0559G                                     01 
          Descriptor          : CAP CER 1uF +/-10% 16V 0402 X6S                        
          Supplier            : Murata                                                 
          Supplier Number     : GRM155C81C105KE11                                      
          Value               : 1uF                                                    
          Max Rating          : 16V                                                    
          Tolerance           : 10%                                                    
          Size                : 0402                                                   
       Capacitor 5            : SID#5B-63-1078G                                     02 
          Descriptor          : CAP CER 1uF +/-10% 16V 0402 X6S                        
          Supplier            : Taiyo Yuden                                            
          Supplier Number     : LMK105C6105KV-F                                        
          Value               : 1uF                                                    
          Max Rating          : 16V                                                    
          Tolerance           : 10%                                                    
          Size                : 0402                                                   
       Capacitor 5 Qty        : 1                                                   01 
       Capacitor 6            : SID#5B-63-1102G                                     01 
          Descriptor          : CAP CER 100nF 10% 25VSMD 0201 GP X6S                   
          Supplier            : Taiyo Yuden                                            
          Supplier Number     : TMK063C6104KP-F                                        
          Value               : 100nF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 10%                                                    
          Size                : 0201                                                   
       Capacitor 6            : SID#5B-63-1062G                                     02 
          Descriptor          : CAP CER 100nF 10% 10V SMD 0201 GP X6S                  
          Supplier            : Walsin                                                 
          Supplier Number     : 0201S104K100CT                                         
          Value               : 100nF                                                  
          Max Rating          : 10V                                                    
          Tolerance           : 10%                                                    
          Size                : 0201                                                   
       Capacitor 6 Qty        : 10                                                  01 
       Capacitor 7            : SID#5B-63-0919G                                     01 
          Descriptor          : CAP CER 6.8pF +/-0.1pF 25V 0201 C0G HF                 
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1E6R8BA01D                                     
          Value               : 6.8pF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 7            : SID#5B-63-1074G                                     02 
          Descriptor          : CAP CER 6.8pF +/-0.1pF 25V 0201 C0G HF                 
          Supplier            : Yageo                                                  
          Supplier Number     : CQ0201BRNPO8BN6R8                                      
          Value               : 6.8pF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 7            : SID#5B-63-1117G                                     03 
          Descriptor          : CAP CER 6.8PF 50V NP0 0201                             
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1H6R8BA01D                                     
          Value               : 6.8pF                                                  
          Max Rating          : 50V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 7 Qty        : 1                                                   01 
       Capacitor 8            : SID#5B-63-0919G                                     01 
          Descriptor          : CAP CER 6.8pF +/-0.1pF 25V 0201 C0G HF                 
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1E6R8BA01D                                     
          Value               : 6.8pF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 8            : SID#5B-63-1074G                                     02 
          Descriptor          : CAP CER 6.8pF +/-0.1pF 25V 0201 C0G HF                 
          Supplier            : Yageo                                                  
          Supplier Number     : CQ0201BRNPO8BN6R8                                      
          Value               : 6.8pF                                                  
          Max Rating          : 25V                                                    
          Size                : 0201                                                   
       Capacitor 8            : SID#5B-63-1118G                                     03 
          Descriptor          : CAP CER 7.5PF 50V C0G/NP0 0201                         
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1H7R5BA01D                                     
          Value               : 7.5pF                                                  
          Max Rating          : 50V                                                    
          Size                : 0201                                                   
       Capacitor 8 Qty        : 1                                                   01 
       Capacitor 9            : SID#5B-63-0921G                                     01 
          Descriptor          : CAP CER 10pF  /-5 50V 0201 C0G HF                      
          Supplier            : Murata                                                 
          Supplier Number     : GRM0335C1H100JA01D                                     
          Value               : 10pF                                                   
          Max Rating          : 50V                                                    
          Tolerance           : 5                                                      
          Size                : 0201                                                   
       Capacitor 9            : SID#5B-63-1072G                                     02 
          Descriptor          : CER SMD GPCAP CER 10pF +/-5% 50V 0201 C0G HF           
          Supplier            : Yageo                                                  
          Supplier Number     : CC0201JRNPO9BN100                                      
          Value               : 10pF                                                   
          Max Rating          : 50V                                                    
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       Capacitor 9 Qty        : 2                                                   01 
       Capacitor 10           : SID#5B-63-0089G                                     01 
          Descriptor          : CAP CER 10nF 10% 25V SMD 0201 GP/HF X7R T=0.3mm        
          Supplier            : Yageo                                                  
          Supplier Number     : CC0201KRX7R7BB103                                      
          Value               : 10nF                                                   
          Max Rating          : 25V                                                    
          Tolerance           : 10%                                                    
          Size                : 0201                                                   
       Capacitor 10           : SID#5B-63-0915G                                     02 
          Descriptor          : CAP 10nF 10% 25V SMD 0201 GP/HF X7R                    
          Supplier            : Murata                                                 
          Supplier Number     : GRM033R71A103KA01D                                     
          Value               : 10nF                                                   
          Max Rating          : 25V                                                    
          Tolerance           : 10%                                                    
          Size                : 0201                                                   
       Capacitor 10 Qty       : 1                                                   01 
       Capacitor 11           : SID#5B-63-1018G                                     01 
          Descriptor          : CAP CER 8.2pF +/-0.1pF 25V SMD 0201 GP/HF C0G          
          Supplier            : Murata                                                 
          Supplier Number     : RM0335C1E8R2BA01D                                      
          Value               : 8.2pF                                                  
          Max Rating          : 25V                                                    
          Tolerance           : 0.1pF                                                  
          Size                : 0201                                                   
       Capacitor 11 Qty       : 1                                                   01 
       Capacitor 12           : SID#5B-63-1021G                                     01 
          Descriptor          : CAP CER 10uF 20% 10V SMD 0603 GP/HF X6S                
          Supplier            : Taiyo Yuden                                            
          Supplier Number     : LMK107BC6106MA-T                                       
          Value               : 10uF                                                   
          Max Rating          : 10V                                                    
          Tolerance           : 20%                                                    
          Size                : 0603                                                   
       Capacitor 12           : SID#5B-63-1015G                                     02 
          Descriptor          : CAP CER 10uF 20% 10V SMD 0603 GP/HF X6S                
          Supplier            : Murata                                                 
          Supplier Number     : GRM188D71A106MA73D                                     
          Value               : 10uF                                                   
          Max Rating          : 10V                                                    
          Tolerance           : 20%                                                    
          Size                : 0603                                                   
       Capacitor 12           : SID#5B-63-1063G                                     03 
          Descriptor          : CAP CER 10uF 20% 10V SMD 0603 GP X7T T=0.8mm           
          Supplier            : TDK                                                    
          Supplier Number     : C1608X6S1A106M080AC                                    
          Value               : 10uF                                                   
          Max Rating          : 10V                                                    
          Tolerance           : 20%                                                    
          Size                : 0603                                                   
       Capacitor 12 Qty       : 3                                                   01 
       Crystal                : SID#5B-69-0046G                                     01 
          Descriptor          : XTAL 40MHz 5ppm 8pF 40ohm SMD GP/HF                    
          Supplier            : TXC                                                    
          Supplier Number     : 8Y40072002                                             
          Value               : 40MHz                                                  
          Max Rating          : 8pF                                                    
          Tolerance           : -3~7ppm                                                
          Size                : 2.0*1.6*0.5                                            
       Crystal                : SID#5B-69-0047G                                     02 
          Descriptor          : XTAL 40MHz 5ppm 8pF 40ohm SMD GP/HF                    
          Supplier            : TXC                                                    
          Supplier Number     : 8Y40072002                                             
          Value               : 40MHz                                                  
          Max Rating          : 8pF                                                    
          Tolerance           : -3~7ppm                                                
          Size                : 2.0*1.6*0.5                                            
       Filter                 : SID#5B-68-0009G                                     01 
          Descriptor          : FILTER C 2400~2500MHz 1.7dB 50ohm 0603                 
          Supplier            : TDK                                                    
          Supplier Number     : DEA202450BT-1294C1-H                                   
          Value               : 2400Mhz                                                
          Max Rating          : 1.7dB                                                  
          Size                : 2.0*1.25*0.8                                           
       Filter                 : SID#5B-68-0012G                                     02 
          Descriptor          : FILTER BPF 2412~2484MHz 1.35dB SMD 0805 GP/HF          
          Supplier            : Walsin                                                 
          Supplier Number     : RFBPF2012080AC2T20                                     
          Value               : 2412Mhz                                                
          Max Rating          : 1.35dB                                                 
          Size                : 0805                                                   
       Filter                 : SID#5B-68-0011G                                     03 
          Descriptor          : FILT D 2400~2500/4900~5950MHz 0.5/0.7dB                
          Supplier            : TDK                                                    
          Supplier Number     : DPX165950DT-8148A1                                     
          Value               : 2400Mhz                                                
          Max Rating          : 0.35dB                                                 
          Size                : 1.6*0.8*0.6                                            
       Inductor               : SID#5B-66-0190G                                     01 
          Descriptor          : IND F 2.2uH 30% 1.2A 0.11ohm 2.0*1.6mm                 
          Supplier            : Murata                                                 
          Supplier Number     : LQM2MPN2R2NG0L                                         
          Value               : 2.2uH                                                  
          Max Rating          : 1.2A                                                   
          Tolerance           : 30%                                                    
          Size                : 2.0*1.6*0.9                                            
       Inductor               : SID#5B-66-0199G                                     02 
          Descriptor          : IND F 2.2uH 30% 1.2A 0.11ohm 2.0*1.6mm                 
          Supplier            : TDK                                                    
          Supplier Number     : MLP2016H2R2MT0S1                                       
          Value               : 2.2uH                                                  
          Max Rating          : 1.2A                                                   
          Tolerance           : 30%                                                    
          Size                : 2.0*1.6*0.9                                            
       Inductor               : SID#5B-66-0202G                                     03 
          Descriptor          : IND F 2.2uH 20% 1.2A 0.11ohm SMD 2.0*1.6mm GP/HF       
          Supplier            : Maglayers                                              
          Supplier Number     : MLN-TP10N2R2M-P4-RU                                    
          Value               : 2.2uH                                                  
          Max Rating          : 1.2A                                                   
          Tolerance           : 20%                                                    
          Size                : 2.0*1.6*0.9                                            
       Inductor Qty           : 2                                                   01 
       Inductor 2             : SID#5B-66-0191G                                     01 
          Descriptor          : IND F 1uH 20% 1.6A 0.055ohm SMD 1008                   
          Supplier            : MURATA                                                 
          Supplier Number     : LQM2HPN1R0MG0L                                         
          Value               : 1uH                                                    
          Max Rating          : 1.6A                                                   
          Tolerance           : 20%                                                    
          Size                : 2.5*2.0*0.9                                            
       Inductor 2             : SID#5B-66-0200G                                     02 
          Descriptor          : IND F 1uH 20% 1.5A 0.100mohm SMD 1008 GP/HF            
          Supplier            : TDK                                                    
          Supplier Number     : MLP2520H1R0MT0S1                                       
          Value               : 1uH                                                    
          Max Rating          : 1.5A                                                   
          Tolerance           : 20%                                                    
          Size                : 2.5*2.0*0.9                                            
       Inductor 2             : SID#5B-66-0197G                                     03 
          Descriptor          : IND F 1uH 20% 1.5A 0.69ohm SMD 1008 GP/HF              
          Supplier            : Maglayers                                              
          Supplier Number     : MLN-YT10N1R0M-XB-RU                                    
          Value               : 1uH                                                    
          Max Rating          : 1.5A                                                   
          Tolerance           : 20%                                                    
          Size                : 1008                                                   
       Inductor 2 Qty         : 1                                                   01 
       Inductor 3             : SID#5B-66-0189G                                     01 
          Descriptor          : IND WW 10uH 20% 700mA 0.364ohm SMD 2520GP/HF T=1       
          Supplier            : TDK                                                    
          Supplier Number     : MLP2520S100MT                                          
          Value               : 10uH                                                   
          Max Rating          : 0.7A                                                   
          Tolerance           : 20%                                                    
          Size                : 2.5*2.0*0.85                                           
       Inductor 3             : SID#5B-66-0201G                                     02 
          Descriptor          : IND WW 10uH 20% 700mA 0.364ohm SMD 2520GP/HF T=1       
          Supplier            : Murata                                                 
          Supplier Number     : DFE252010F-100M=P2                                     
          Value               : 10uH                                                   
          Max Rating          : 0.7A                                                   
          Tolerance           : 20%                                                    
          Size                : 2520                                                   
       Inductor 3             : SID#5B-66-0198G                                     03 
          Descriptor          : IND WW 10uH 20% 700mA 0.364ohm SMD 2520GP/HF T=1       
          Supplier            : Maglayers                                              
          Supplier Number     : MLH-YT10N100M-P4-RU                                    
          Value               : 10uH                                                   
          Max Rating          : 0.7A                                                   
          Tolerance           : 20%                                                    
          Size                : 2520                                                   
       Inductor 3 Qty         : 1                                                   01 
       Memory                 : SID#5B-61-0418G                                     01 
          Descriptor          : Serial flash 32Mbit                                    
          Size                : 4*3*0.55                                               
          Supplier            : Macronix                                               
          Supplier Number     : MX25R3235FZBJL0                                        
       Resistor               : SID#5B-62-1153G                                     02 
          Descriptor          : RES C SMD 0201 100Kohm 5% GP/HF                        
          Supplier            : YAGEO                                                  
          Supplier Number     : RC0201JR-07100KP                                       
          Value               : 100Kohm                                                
          Max Rating          : 1/20W                                                  
          Tolerance           : 5%                                                     
          Size                : 0201                                                   
       RF Switch              : SID#5B-61-0422G                                     02 
          Descriptor          : 20 MHz-6.0 GHz GaAs SPDT Switch                        
          Supplier            : Skyworks                                               
          Supplier Number     : SKY13587-378LF                                         
          Value               : 6GHz                                                   
       RF Switch Qty          : 1                                                   01 
       Filter 3               : SID#5B-68-0011G                                     01 
          Descriptor          : FILT D 2400~2500/4900~5950MHz 0.5/0.7dB                
          Supplier            : TDK                                                    
          Supplier Number     : DPX165950DT-8148A1                                     
          Value               : 2400Mhz                                                
          Max Rating          : 0.35dB                                                 
          Size                : 1.6*0.8*0.6                                            
       Filter 3               : SID#5B-68-0013G                                     02 
          Descriptor          : FLT D 2400~2500/4900~5950MHz 0.5/0.7dB SMD 0603 GP     
          Supplier            : Walsin                                                 
          Supplier Number     : RFDIP160806LC2T20                                      
          Value               : 2400MHz                                                
          Max Rating          : 0.7dB                                                  
          Size                : 0603                                                   
       Filter 3 Qty           : 1                                                   01 
       Crystal Qty            : 1                                                   01 
       Crystal 2              : SID#5B-69-0042G                                     01 
          Designator          : XT2
          Descriptor          : XTAL 32.768KHz 20ppm 7pF 70Kohm SMD GP                 
          Supplier            : TXC                                                    
          Supplier Number     : 9H03270072                                             
          Value               : 32.768KHz                                              
          Max Rating          : 7pF                                                    
          Tolerance           : 20%                                                    
          Size                : 3.2*1.5*0.75                                           
       Crystal 2              : SID#5B-69-0045G                                     02 
          Designator          : XT1
          Descriptor          : XTAL 40MHz 5ppm 8pF 40ohm SMD GP/HF                    
          Value               : 40MHz                                                  
          Max Rating          : 8pF                                                    
          Tolerance           : -3~7ppm                                                
          Size                : 2.0*1.6*0.5                                            
       Crystal 2 Qty          : 1                                                   01 
    
    TS17586AC0_7358-D_GEN3.pdf

    For the BD, is it possible to show them section 4 of the DS: https://www.ti.com/lit/ds/symlink/cc3235modasf.pdf?ts=1769611107065&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FCC3235MODASF

    Hopefully this covers what they need. As always, let me know how else I can help.

    Best,

    Josh

  • Hi Josh,

    Sorry to interrupt. My name is Sumin, and I am responsible for TI wifi module KC certification in Korea team. The KC testing laboratory has requested the following information. Could you please review the request and provide the relevant details at your earliest convenience?

    1. Frequency bandwidth of the Wi-fi module (e.g. 2.45GHz band (2402MHz ~ 2483.5MHz) or 5GHz band (5150MHz ~ 5850MHz))
    2. Mode for Wi-fi module (e.g. 802.11a/b/g/n20/n40/ac20/ac40/ac80, etc.)
    3. Target output power or Power tolerance of the Wi-fi module
    4. Whether SISO or MIMO operating configuration

    Thanks in advance.

    Best regards,

    Sumin

  • Hi Sumin,

    IEEE 802.11a/b/g/n/ac part:

    - Operating frequency range: 2400.0 to 2483.5 MHz 

              - EIRP: < 20 dBm

    - Operating frequency range: 5150 to 5350 MHz (indoor use only) / 5500 to 5725 MHz

              - EIRP: < 23 dBm

    SISO only.

     Best,

    Josh

  • Hi Josh,

    Wish you all the best.!

    I have a new request. Could you please provide me with the detailed specifications of the PCB antenna? I found some information in the 8.10 section of the datasheet, but it only contained polarity, peak gain, and efficiency data.

    Kind regards,

    Kyrin

  • Hi Kyrin,

    What specifically are you looking for? Which other antenna data?

    Josh

  • Hi Josh,

    The specific parameters are as follows:

    V.S.W.R, return loss, radiation patterns and corresponding peak gain values. 

    Information similar to that shown in the link below would be helpful.

    photos.app.goo.gl/NZE4qu7vT7ch9Hrx9

    Kind regards,

    Kyrin

  • Hey Kyrin,

    Could you email connectivity-wifi-cert@list.ti.com with this request so I can service you there? The material you are requesting is sensitive. Do we have NDA with you all?

    Josh

  • Hi Josh,

    I have sent the email, please help follow up on the content of the email. Thank you.

    Kind regards,

    Kyrin