We are using the WL1271 with WPA under linux.
If the SSID is being broadcast we can go out of range and come back into range and the WL1271
properly re-associates with the access point.
But if the SSID is not being broadcast re-association does not ever occur.
We must restart the system or driver to get the connection back.
We also see this same behavior with a commercial android tablet that uses the WL1271.
Is this a known issue ? Is there a work-around/fix ?