I am trying to place my Wifi Module (Murata LBEH19XMMC which uses TI's WL1271) in continuous transmit mode for FCC testing, but the it seems that the module does not output a constant RF signal. My FCC test lab tells me that the transmission is bursty and not continuous "We would get a couple of milliseconds of transmission and then nothing. Even this didn’t appear to be timed to our execution of the commands."
The FCC test lab seems to be using the correct command sequence per TI, they are using the procedures and commands in section 14.7 page 120 of the WL1271 CLI documents.
/ w p 1 f 2
/ t r h 0 11
/ t r t n 2000 4096 1000 0 16375 0 3 0 0 4 0 0 1 1 11:22:33:44:55:66
This is a WInCE environment using Ticon.exe.
Can anyone help? I imagine that someone must have taken this module to through FCC testing procedures.