A customer uses a competitors module in a battery application that transmits very little data. Key for the application is low power. To achieve low power they only apply power to the module when they want to transmit data; from power on (this is just the module), connect to the network, transmit the data (maybe 10 bytes?), to power down takes about 2 seconds. Any idea what the CC3000 can do? Another option might be to leave the CC3000 in low power standby and do the same thing from there, any idea how long that would take?