This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1271/73 packet loss issue.

Other Parts Discussed in Thread: AM3505, WL1271

Hi,

I am using WL1271/73 with AM3505. We want both ethernet and wifi running simultaneously.

What I observed is the ethernet works fine (0% packet loss, testing with iperf) with ~25Mbps full duplex.

When the ethernet test is running and I start the Wifi (iwconfig tiwlan0 up) I see 100% packet loss on ethernet.

If I disable the wifi (iwconfig tiwlan0 down) I again see 0% packet loss on ethernet. So I feel the wifi is causing the ethernet packet loss.

Has anyone encountered such problem? If yes, what can be the problem here?

Regards,

Krunal