This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3551E: Simplelink-WiFi-Toolbox versions

Part Number: CC3551E
Other Parts Discussed in Thread: SIMPLELINK-WIFI-TOOLBOX

Hi,

 

I have today version 4.1.8 of the Simplelink-WiFi-Toolbox  installed on my computer. My question is regarding then it comes a new update of the Simplelink-WiFi-Toolbox, i.e., let us say the new version  is 4.1.9:

  1. Can then one install this new version 4.1.9 without uninstalling the previous version 4.1.8?
  2. This would mean that the existing version 4.1.8 is installed under "C:\ti\simplelink_wifi_toolbox_win_4_1_8" can continue to work as before after the new version has been installed under "C:\ti\simplelink_wifi_toolbox_win_4_1_9"?

BR

Håkan

  • Hi Håkan,

    Can then one install this new version 4.1.9 without uninstalling the previous version 4.1.8?

    This is correct, you do not need to uninstall previous versions. 

    This would mean that the existing version 4.1.8 is installed under "C:\ti\simplelink_wifi_toolbox_win_4_1_8" can continue to work as before after the new version has been installed under "C:\ti\simplelink_wifi_toolbox_win_4_1_9"?

    This is correct, both versions of the toolbox will continue to function regardless of other versions of the toolboxes downloaded.

    Let me know if you have any additional questions!

    Best Regards,

    Josh Prushing