Part Number: WL1835MOD
Other Parts Discussed in Thread: WL1837MOD, WL1835,
Hello,
We are using the WL1835MODGBMOCR in a Linux-based embedded product (Yocto / NXP iMX8) and are currently pursuing certification in China.
We are failing the adaptive interference avoidance test (2.4 GHz, STA mode) under MIIT 2021 No. 129. From our understanding, the test requires the device to autonomously detect channel occupation and halt transmission without external intervention. Our device continues transmitting when an interferer fully occupies the connected channel.
We have three specific questions:
1. SRRC certification status: We are aware from a prior E2E thread (WL1837MOD, thread #1278121) that TI "cannot confirm whether or not WL1837MOD is compliant with SRRC certification because TI has not done the certification process". Is this still actual? Is there any new development or planned timeline?
2. Firmware-level DAA/LBT capability: Does the WL1835 firmware (wl18xx-fw-4.bin) implement any Listen Before Talk (LBT) or Detect And Avoid (DAA) mechanism autonomously, or is interference avoidance entirely delegated to the host stack (mac80211 / wpa_supplicant)?
Any guidance, would be very helpful.
Thank you.