Hi, I am l looking at using the LSR TIWI-R2 with AM335X Chip set. My issue is that this will be a headless device and I would like to start the board in WLAN router configuration and have it create an ad-hoc network so a mobile device can see it and join it. Once the mobile device is joined, it would then configure the board to connect to a secure WLAN already existing. Once the configurations are in the board, it will reset and join the secure WLAN you told it to. I would like to know if this is possible, if so, are there any samples of this in place today?
Any Help will be appreciated!