Other Parts Discussed in Thread: MSP430FR5739
I am having difficulty getting this simple web server application to operate correctly. I downloaded the application from the TI wiki ( http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads ). Had a little difficulty with CCS V5 importing the project as there is a bad file pointer for the Sensor.C file. Managed to get through all that. Build and download was successful. Here is where I have some problems.
I was unable to get First-Time-Config to work properly. I would get led1, led2 and Led3 to light, but no led4. If I press the reset button (or restart my debug session) the process starts all over again. (works fine for default sensor app)
I modified Demo_Config.H by adding my SSID #define DEFAULT_OUT_OF_BOX_SSID "TP-LINK_2CDBE4"
Now when the board starts up, it connects to my router automatically - LEDS1-4 are lit. On to the next issue - serving up the web page. If I point my browser (firefox) to the correct IP address (http://192.168.1.100) I get nothing, it just times out. If I use port 81 (i saw something in the code) which is http://192.168.1.100:81 the FRAM board immediately drops the link and resets once or twice.
Can someone at TI please walk the E2E community through the process of getting this demo application example running on our hardware. If there is new code, please publish here or on the wiki.
Please verify that it will actually serve up some sort of web page.
I know this is an issue for more than one of us. Thanks.