CC3501E: Python script for a automated testing

Part Number: CC3501E
Other Parts Discussed in Thread: SIMPLELINK-WIFI-TOOLBOX

All, 

My assigned focus customer is working on factory testing.  They ask:

I’m currently creating a python script to automate running through a flash check, RF CCW test and GPIO connectivity/short test.  First two are working fine but can’t seem to get GPIO commands to work.

 

This is an example of what I thought would work but get a timeout error.

 

PS C:\ti\simplelink_wifi_toolbox_win_4_3_23> ./simplelink-wifi-toolbox radio-tool -i XDS110 -param1 LS420BFL common io_mux cc35xxe_set --io_id GPIO16 --io_direction OUTPUT --io_state HIGH

 

I dropped back to testing this on the Launchpad demo board using the XDS110ET interface. 

Do you have any guidance or solid examples I can use?