4338.TI_TP_ACS_BI-14-I.zipHello,
We are developing device based on WL1273.
We have problem with BQB HFP test TP/ACS/BI-14-I.
Our device has the AG role.
The HF (simulated by the PTS dongle) requests to establish eSCO connection with invalid Transmit_Bandwidth and invalid Receive_Bandwidthparameters (12000bytes/sec instead of 8000bytes/sec).
Those two parameters will be translated later by the Host and will be transferred to the BT chip (at AG device side) via HCI command HCI_Setup_Synchronous_Connection (opcode 0x0428).
Enclosed please find: FTS_ACS_BI-14-I_Sniffer_failed.cfa - Air sniffer log.
We would like to find out which BT command (packet) being transferred from HF to AG via the air interface contains the Transmit bandwidth and Receive bandwidth parameters.