Hello ,
I am presently trying to interface the HOST PC via UART motherboard with Murata_board (LBEH59XUHC ).I configured the hardware using the Murata_LBEH59XUHC test manual.
when i use the hciattach command I get the following response "request timed out."
I would like to know is there any possiblity to check whether the BT_Enable bit is set i could see the BT_WAKEUP pin being maintained at 0v
also the UART communication between the motherboard and the daughter board is fine.
when i try to run the demo scripts its throwing an error "Can't get device info no such device"
Any information in this would be of great help