Hi,
When I test spurious emission of CC3000 on 2.4GHz-3.4GHz, how to set RBW and VBW ? When I set RBW=1MHz, the test result will exceed
the criterion. And what is the standard of RBW on spurious emission?
Look forword to your answer. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lei,
What is your test setup like? From experience, I have seen that the instruments you are using come with application notes and in some cases even small applications that do the whole job for you by automating the configurations of your test setup. That being said, I am not sure if there are settings specific to the CC3000 module. I know for a fact that most standards on in-band and out-of-band spurious emissions are from IEEE or FCC.
As per the TiWi-SL Module Datasheet, it complies with FCC standard; FCC ID: TFB -TIWISL01, 15.247 (Page 32 of the Datasheet).
Read FCC Standard: 15.247 (You should be able to find this on the internet).