This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 SimpleLink Library Timeout

Is there a way to change the time out time of the TiWi? Or do I have to do it manually. 

When I call recv(), the tiwi has a very long timeout.  In the API there is there setsockopt(), but the timeout option is not supported. 

I can have my own timer with an interrupt on the MSP, that when triggered, deasserts the power enable on the TiWi, but then I will have to reconnect to the network again.

Is there a simpler way?  Is the TiWi itself hanging, or is it just the API code?  That is, if my shorter timeout happens, could I just issue another command to the TiWi instead?

Thanks,

Nathan