This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EXP430FR5739 Sensor Application

Hi

I want to make my Experimenter Board EXP430FR5739 work with the CC3000 FRAM Sensor Application.

My computer has WinXP Professional Version 2002 Service Pack 3, the firewall is (for this purpose) disabled.

The router is TP-Link Model TL-WR740N, connected to the PC.

The Experimenter Board has an LSR module model TiWi-SL Ref.2 and is connected to the same PC and accessible via COM4.

I can access the Experimenter Board by a monitor program. With "assoc TP-LINK_######" I get the response

Sensor App Version: v1.0.7
WLAN Enabled
Attempting to connect using SSID: TP-LINK_######
Connected to AP: TP-LINK_######
CC3000 MAC Address: ##:##:##:##:##:##
CC3000 IP Address: 192.168.1.101
Starting Server...
Server Initialized on port 1204
Waiting for Clients

The last two lines are repeated every minute. LEDs 1-4 are on.

When I connect to the router with a browser via http://192.168.1.1/, I see under "DHCP --> DHCP Clients list" the MAC and IP of my PC and the Experimenter Board. The board has IP 192.168.1.101. Under "IP & MAC Binding --> Binding Settings" I see the same devices with the same MAC and IP. Under "IP & MAC Binding --> ARP List" I only the MAC and IP of my PC. Under "Wireless --> Wireless Statistics" I see both devices with their MAC Addresses and the number of received and sent packets.

When I now disconnect COM4 from the monitor program and start the CC3000 FRAM Sensor GUI, I press the "Continue" button at the "Automatic Configuration" message box. The program finds the board under COM4 ("Configuration Successful") and opens the "CC3000SensorAppGUI" window. The application does not communicate with the Experimenter Board ("0 Nodes Connected") and after a time a message box appears "A CC3000 device has not been found on the network" etc.

Again looking to the browser under "Wireless Statistics" I see that there are packets sent and received in regular intervals.

So were could be the problem?

Thanks, Bert