Issue:
We are using LSR TiWi-R2 module with WL1271 chip. The module performs correctly as WLAN interface under Linux. When we ready signal power level for all access points in the area, thoses the closest show no mor ethan -45 dB level with constant fluctuations to -65db or even -85 dB. These readings are off by -20 dB from other Wifi receivers ( Laptops with Windows) and even when reading with specialized WLAN test software.
We followed teh calibration procedure provided by LSR/TI to no change.
Question:
We would like to read noise power level but full data sheet for this device is not available and we do nto knwo which register may have this value.
Help on both questions will be appreciated