Hi.
When I use the IAR Embeded Workbench IDE(5.40.3) to debug the CC3000+FRAM Basic WiFi Application , Typing the command,for example 02 03 06 04 and so on. Everything is normal, I can receive some data from FRAM Board with CC3000. But, When power off, then power on ,that is exit the debug mode. then I type the same command ,the board does not have any reaction, LED8 is always off, Why?