HI
In android ICS menu, it is showing that AP is up. But any stations are not able to connect to it. Even for wl1271 station mode it is not able to connect to any of the access points around. If the AP is in open mode wl1271 may associate with it. But it will disconnect within 2-4 seconds. What might be the problem. Calibration issues? or SDIO interfaces problem?
REGARDS
pradeep kumar.M