This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3000 Patch Programming Failure

I compiled both the Driver Patch Programmer and Firmware Patch Programmer.

Before running either of these I ran nvmem_read_sp_version which returned 1.7  I also ran nvmem_get_mac_address and it seemed to return a valid IP MAC address.

I ran the Driver Patch Programmer first.  It ran just fine.

I then ran the Firmware Patch Programmer.  LED #5 came on for several seconds, then blinked off.  No other LEDS came on.  The power light stayed on the entire time, but no other LEDS came on.  I waited for several minutes, then powered the board off.

Now when I run the Basic Wifi Application, wlan_start never returns.  I can't read the nvmem_read_sp_version.

Is there anything I can do?  Hopefully someone can help me!