Hello,
I'm testing a COM6L-T5 module on the AM335x EVM. I'm running some tests to figure out the performances of the bluetooth connection to a PC running Linux (Mint 13) with a USB-Bluetooth adapter (class 2 + EDR). The AM335x EVM and the PC are in line of sight (distance < 50 cm).
I run two tests:
1) Obexftp file transfer. I run the "obexftpd" server on one side and a "obexftp put" on the other side. With this test I get about 65 kbyte/s as transfer rate (both from pc to evm and evm to pc).
2) L2CAP layer speed test. I run the l2test program on both sides (one listening, the other sending) and I get about 200 kbyte/s from evm to pc and about 260 kbyte/s from pc to evm.
In your experience, are these figures reasonable? Can you suggest other tests I can run for bluetooth throughput measurement?
Thanks for your help.
Best Regards,
Piero