This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Changing the channel of a wl1273 operating as an AP

Other Parts Discussed in Thread: WL1271

I have an wl1273 running as AP (using hostapd)

  I want to change the channel used by the AP

I tried

iw wlan0 set channel 2

but got

         command failed: Device or resource busy (-16)

Have people successfully run this command?

Is there another way of doing this ?

Re-starting hostapd with a different config file seem highly inefficient ...

thanks

Bernard

----
Details

Processor : 8148

WIFI chip : 1273

Driver : "R4_SP2_02_04"

Firmware : 6.3.0.72.77

Kernel : 2.6.37