This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Basic Wi-Fi example application for Launchpad - cannot start it

Other Parts Discussed in Thread: MSP430F2132

I am using the EVM and launchpad G2. I have loaded the Patch Programmer Installer and ran it so both driver and firmware are loaded. I also waited 30 seconds after each. I then set up Hyperterminal as instructed and removed power from the boards. I then re-powered them but got nothing on the screen. It refers to a Stellaris board but also says that the first digit refers to which MCU is used. Can anyone help with suggestions?

Thanks

Peter