This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3000 wifi chip



Hello,

I am using cc3000. it needs a power supply 250mA. Can I use TPS77333 voltage regulator because It supplies 3.3V output and 250mA. 3.3 voltage has enough to operate cc3000 or 3.6V? Another thing is that I supply a 2.5V to msp430, then VIO_HOST cc3000 also 2.5V, while VBAT cc3000 is 3.3V. That means VIO_HOST = 2.5V and VBAT = 3.3V. Does it work?

Thanks