This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unhandled event causes the stack to hang.....

I am writing a json client that makes a lot of json POSTs and receives json data back from a server. I have had a lot of problems getting the stack to perform reliably for any lengthy time so I decided to see what was going on.

To make a (very) long story short it seems that I suddenly get a SEND reply with the status set to -1. Looking in the code I could see that this is not handled at all and leaves the system with interrupts disabled and unresponsive. It seems the stack handles -57 as ERROR_SOCKET_INACTIVE in the evnt_handler so I decided to try and handle -1 the same way and low and behold that seem to have solved most of my problems.

                pArg = M_BSD_RESP_PARAMS_OFFSET(event_hdr);
                STREAM_TO_UINT32(pArg, BSD_RSP_PARAMS_STATUS_OFFSET,status);
                
                if (ERROR_SOCKET_INACTIVE == status || -1 == status)  // My changed line
                {
                    // The only synchronous event that can come from SL device in form of 
                    // command complete is "Command Complete" on data sent, in case SL device 

The system still hangs (much less though) but this looks like it is another problem. I will dig into that next.

I am running 1.11.1 on host and module (1.24).

It would be great to have some sort of confirmation or comment from TI guys on this. I'm not sure if this is a bug in the FW, the host software or if I am doing something else incorrectly.

/P