This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP Linux 3.4.68 wl12xx: ERROR command complete timeout

Other Parts Discussed in Thread: WL1271, OMAP3530

Hello, we are using Linux 3.4.68 and the included wl12xx_stio driver with 6.3.5.0.98 firmware on our OMAP3 board. 

We are using ConnMan 1.19 and Wpa_Supplicant 2.0 to connect to a WiFi router. The association eventually succeeds and internet connectivity is achieved and maintained, however, we always receive this error:

wl12xx: ERROR command complete timeout

at the beginning of association. The driver then seemingly must reset itself several times:

wl12xx: ERROR watchdog interrupt received! starting recovery

Finally, the association is completed and all is well.

What could cause these issues and how can I fix them? Thanks!

I've pasted the dmesg output and also the output of cat /proc/interrupts below. I appreciate your help.

=== DMESG:

wl12xx: loaded

wl12xx: firmware booted (Rev 6.3.5.0.98)

wlan0: authenticate with 2c:b0:5d:a8:fc:50

wlan0: send auth to 2c:b0:5d:a8:fc:50 (try 1/3)

wlan0: authenticated

wlan0: associate with 2c:b0:5d:a8:fc:50 (try 1/3)

wlan0: RX AssocResp from 2c:b0:5d:a8:fc:50 (capab=0x431 status=0 aid=1)

wl12xx: ERROR command complete timeout

------------[ cut here ]------------

WARNING: at drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x318/0x348()

Modules linked in: wl12xx_sdio lpm_omap3530(O) twl4030_keypad_fluke dsplinkk(O) twl4030_pwrbutton sdmak(O) cmemk(O) [last unloaded: wl12xx_sdio]

[<c00133b4>] (unwind_backtrace+0x0/0x11c) from [<c003072c>] (warn_slowpath_common+0x4c/0x64)

[<c003072c>] (warn_slowpath_common+0x4c/0x64) from [<c003075c>] (warn_slowpath_null+0x18/0x1c)

[<c003075c>] (warn_slowpath_null+0x18/0x1c) from [<c023f7c8>] (wl1271_cmd_send+0x318/0x348)

[<c023f7c8>] (wl1271_cmd_send+0x318/0x348) from [<c0240d8c>] (wl1271_cmd_configure+0x70/0xa0)

[<c0240d8c>] (wl1271_cmd_configure+0x70/0xa0) from [<c02482e0>] (wl1271_acx_set_ht_capabilities+0xc8/0x108)

omap3isp omap3isp: CCDC won't become idle!

[<c02482e0>] (wl1271_acx_set_ht_capabilities+0xc8/0x108) from [<c023d054>] (wl1271_op_bss_info_changed+0xb08/0xc88)

[<c023d054>] (wl1271_op_bss_info_changed+0xb08/0xc88) from [<c0395634>] (ieee80211_bss_info_change_notify+0x1a0/0x278)

[<c0395634>] (ieee80211_bss_info_change_notify+0x1a0/0x278) from [<c03d5c04>] (ieee80211_assoc_success+0x398/0x544)

[<c03d5c04>] (ieee80211_assoc_success+0x398/0x544) from [<c03c547c>] (ieee80211_rx_mgmt_assoc_resp+0x1ac/0x214)

[<c03c547c>] (ieee80211_rx_mgmt_assoc_resp+0x1ac/0x214) from [<c03c5960>] (ieee80211_sta_rx_queued_mgmt+0x410/0x524)

[<c03c5960>] (ieee80211_sta_rx_queued_mgmt+0x410/0x524) from [<c03a1c68>] (ieee80211_iface_work+0x200/0x284)

[<c03a1c68>] (ieee80211_iface_work+0x200/0x284) from [<c00484f0>] (process_one_work+0x260/0x47c)

[<c00484f0>] (process_one_work+0x260/0x47c) from [<c0048904>] (worker_thread+0x1cc/0x310)

[<c0048904>] (worker_thread+0x1cc/0x310) from [<c004d158>] (kthread+0x80/0x90)

omap3isp omap3isp: CCDC won't become idle!

[<c004d158>] (kthread+0x80/0x90) from [<c000f0c8>] (kernel_thread_exit+0x0/0x8)

---[ end trace 1b75b31a2719ed33 ]---

wl12xx: WARNING CONFIGURE command NOK

wl12xx: WARNING acx ht capabilities setting failed: -110

wl12xx: WARNING Set ht cap true failed -110

wl12xx: ERROR watchdog interrupt received! starting recovery.

wlan0: associated

wl12xx: Reading FW panic log

wl12xx: ERROR command complete timeout

------------[ cut here ]------------

WARNING: at drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x318/0x348()

Modules linked in: wl12xx_sdio lpm_omap3530(O) twl4030_keypad_fluke dsplinkk(O) twl4030_pwrbutton sdmak(O) cmemk(O) [last unloaded: wl12xx_sdio]

[<c00133b4>] (unwind_backtrace+0x0/0x11c) from [<c003072c>] (warn_slowpath_common+0x4c/0x64)

omap3isp omap3isp: CCDC won't become idle!

[<c003072c>] (warn_slowpath_common+0x4c/0x64) from [<c003075c>] (warn_slowpath_null+0x18/0x1c)

[<c003075c>] (warn_slowpath_null+0x18/0x1c) from [<c023f7c8>] (wl1271_cmd_send+0x318/0x348)

[<c023f7c8>] (wl1271_cmd_send+0x318/0x348) from [<c02421a8>] (wl12xx_cmd_stop_fwlog+0x80/0xbc)

[<c02421a8>] (wl12xx_cmd_stop_fwlog+0x80/0xbc) from [<c023e26c>] (wl1271_recovery_work+0xb8/0x308)

[<c023e26c>] (wl1271_recovery_work+0xb8/0x308) from [<c00484f0>] (process_one_work+0x260/0x47c)

[<c00484f0>] (process_one_work+0x260/0x47c) from [<c0048904>] (worker_thread+0x1cc/0x310)

[<c0048904>] (worker_thread+0x1cc/0x310) from [<c004d158>] (kthread+0x80/0x90)

[<c004d158>] (kthread+0x80/0x90) from [<c000f0c8>] (kernel_thread_exit+0x0/0x8)

---[ end trace 1b75b31a2719ed34 ]---

wl12xx: ERROR failed to send stop firmware logger command

wl12xx: Hardware recovery in progress. FW ver: Rev 6.3.5.0.98 pc: 0x9a16

omap3isp omap3isp: CCDC won't become idle!

wl12xx: down

ieee80211 phy5: Hardware restart was requested

wl12xx: firmware booted (Rev 6.3.5.0.98)

wl12xx: Association completed.

 

# cat /proc/inte*

           CPU0

  7:          0      INTC  TWL4030-PIH

  9:          0      INTC  l3-debug-irq

 10:          1      INTC  l3-app-irq

 12:     135932      INTC  DMA

 20:          0      INTC  gpmc

 24:     564763      INTC  omap-iommu.0, OMAP3 ISP

 25:     169880      INTC  OMAP DISPC

 26:          3      INTC  DSPLINK

 28:          0      INTC  DSPLINK

 37:     283523      INTC  gp timer

 56:      33255      INTC  omap_i2c

 57:     531735      INTC  omap_i2c

 61:      24086      INTC  omap_i2c

 74:        661      INTC  OMAP UART2

 77:      64218      INTC  ehci_hcd:usb1

 83:        554      INTC  mmc1

 86:       3153      INTC  mmc2

 92:          1      INTC  musb-hdrc

 94:      30722      INTC  mmc0

112:        270      GPIO  atmel_mxt_ts

117:        627      GPIO  wl12xx

118:          1      GPIO

152:          0      GPIO  gpiolib

157:        403      GPIO  gpiolib

158:          1      GPIO  gpiolib

288:        530      PRCM  pm_wkup

297:          0      PRCM  hwmod_io, pm_io

320:          0   twl4030  twl4030_gpio

321:          0   twl4030  twl4030_keypad

325:          0   twl4030  twl4030_power

328:          0   twl4030  twl4030_pwrbutton

331:          0   twl4030  rtc0

336:          0   twl4030  mmc1

Err:          0